Skip to main content

Biocoop

Boulazac, France

bg-image

Biocoop is a leader in organic food distribution, with a network of over 500 organic stores. In 2017, a Biocoop franchisee with a number of shops and restaurants in the Aquitaine region, decided to open a new butchery and charcuterie processing laboratory at Boulazac in the Dordogne.

"We have always had great confidence in Daikin technologies. Their engineers are always able to find technological solutions capable of accommodating any environment."

- Sébastien Toulouse, Froid Cuisine 24

CO₂ system

bg-image

As a long-standing customer of installer Froid Cuisine 24, the franchisee sought the company’s help in researching and installing a refrigeration solution for the 1,200 square metre laboratory. A Daikin partner since the installer company’s inception 20 years ago, Froid Cuisine 24 initially suggested Daikin’s ZEAS refrigeration solution. With several Daikin installations already in place, the franchisee was very satisfied with the company. Additionally, the ZEAS solution was one with which Froid Cuisine 24 had a lot of experience.

However, with increasingly strict regulations on the use of higher GWP refrigerants and wishing to follow the Biocoop philosophy on sustainable development, it was decided to opt for an alternative that used CO2, which as a natural refrigerant has no impact on global warming, despite the additional cost of the equipment and its installation compared to a traditional system.

Minimal changes compared to conventional installations

minor changes needed in comparison to a traditional refrigeration solution

The managers of Froid Cuisine 24, new to Tewis transcritical technology, visited a similar installation and the Tewis factory itself, which gave them the confidence in opting for a Tewis system.

A second visit in advance of the installation process focused on critical points including piping for the transcritical CO2 technology. This offered additional reassurance, given the relatively minor changes needed in comparison to a traditional refrigeration solution.

Froid Cuisine 24 has additionally demonstrated its commitment to service support, by obtaining the necessary specialist qualifications and setting up an on-call system for weekends.

Safe, effective and energy efficient

Within the laboratory, there are varying requirements for temperature control, spread across eleven different areas. The Tewis/Daikin 78.3 kW transcritical system provides positive cooling (0 to +2°C in some rooms and +8 to +10°C in others) to meet a range of needs throughout. Thirteen 1.8 kW to 10.5 kW evaporators (one/two per room) are directly connected to the transcritical system, while a second, insulated R-452 system was chosen to provide refrigeration in a separate cool room. An air treatment system using a ducted network provides air conditioning to corridors in the laboratory.

CO2 Safe, effective and energy efficient

In the casings preparation room, where corrosive products in use posed a potential risk to the CO2, an alternative system operating on R-134A refrigerant was installed.

Additionally, a water/CO2 exchanger was installed to provide the chilled water needed in the two dryer and oven areas, as well as a 25 kW CO2/glycoled water exchanger. A 50 kW, 20/45°C water desuperheater has also been integrated with the Tewis system to recover heat, providing domestic hot water and compensating for kitchen ventilation as required.

To ensure maximum safety, CO2 leak detectors have been fitted to all laboratory equipment. These are connected to an audible and visible alarm system which sends automatic alerts by email and SMS.

A communication gateway runs from the transcritical system to each evaporator, connected via a central management system from PC to laboratory, to Froid Cuisine and Tewis.

Learn more

Our other cases

  • ACTION

    As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.
  • Action reclaimed refrigerant allocation

    Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.
  • Biocoop

    Daikin completes the installation and commissioning of the first transcritical CO2 refrigeration solution on the French market at a meat processing laboratory in the Dordogne.
  • C&A

    Looking to renovate its entire HVAC system, the CA store wanted to achieve year-round comfort in the most cost-effective and efficient way.
  • City Centre Hotel

    Chiller change boosts comfort at central London hotel.
  • Claerhout Office

    Advertising agency Claerhout Communication House opted for our VRV IV total solution for their new open landscape office building which provides office space for 45 employees and a conference room for 150 guests.
  • Coral betting office

    Discover how our auto-cleaning roundflow cassettes achieved 50 more energy savings for Coral betting offices.
  • Courtyard Hotel Paris

    The Courtyard conversion marks a successful collaboration between forward- looking urban regeneration and Daikin’s flexible, future-proof VRV heat recovery technology.
  • Crédit Agricole

    Known as "the green bank" due to its agricultural history, Crédit Agricole wanted an energy efficient and low maintenance air conditioning solution for one of its branches.
  • Crystal Tower

    To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution.
  • Holcim cement plant

    The Holcim cement plant relies on state-of-the-art technology to achieve its ambitious environmental and energy-efficiency goals.
  • Ibis Budget Hotel, Ghent

    In March 2018, the new IBIS budget hotel opened its doors at the Dampoort in Ghent, offering guests outstanding comfort in a modern attractive setting. For the building owner Viktor De Maertelaere, investment in an energy efficient and reliable climate control system was key to the budget hotel concept.
  • Immogra

    Daikin’s VRV IV system delivers modern aesthetics with invisible integration of HVAC.
  • JBC

    In its ongoing search to optimise running costs, JBC conducted a site trial with Daikin designed to evaluate the gains generated by Variable Refrigerant Temperature VRT technology.
  • K-Way

    When high-end clothing retailer K-Way opened a new store in Covet Garden, London, we worked with nation-wide D1 contractor Royale to devise and install the perfect energy-efficient solution for the property.
  • Leon's restaurant

    M&E contractor, Synecore, installed its first ‘invisible’ HVAC system, the Daikin VRV IV i-Series at Leon Restaurant, central London, to overcome tight space restrictions and achieve maximum climate control efficiency.
  • Naturkost Brinkman

    Organic specialist retailer Naturkost Brinkman uses Daikin retail refrigeration to deliver improved energy efficiency and in-store comfort.
  • Pomme d'Or Hotel

    Air conditioning has become the norm in most new and refurbished hotels. Today’s systems keep guests cool during summer – and additionally provide cost-efficient heating during winter periods. Daikin heat pumps use renewable energy to do this, cutting hotel operating costs. And there’s also a positive impact on indoor aesthetics.
  • Hotel Santos Porta Fira

    The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.
  • The Post Hotel

    As climate control specialists, we chose our VRV system for the Post Hotel Ghent for its combination of energy-efficient technology and ability to provide more comfort.
  • Radisson Blu and Proximus

    The new Radisson Blue hotel in Bruges is located near Bruges station, an area which has seen extensive redevelopment over the past few years. Built by Belgian property developer Group GL, the impressive new tower complex houses not only the new hotel but also a 6,000 square metre area of office space, currently occupied by GL tenant Proximus.
  • Samrya 44

    With 44 floors of elegantly-designed luxury suites, Samrya 44 adheres only to the highest standards in construction and HVAC.
  • Sportisimo

    For this project, we chose to install an outdoor system that connects to a variety of indoor and ventilation units strategically placed in the shop.
  • The Bloomsbury Hotel

    The VRVIII Heat Recovery System from Daikin was selected for its supremely low energy consumption and ability to off er massive savings in comparison with similar systems
  • THE VYRA HOTEL SUITES

  • Torre Serenissima

    Equipped with an outdated R-22 refrigerant system, we gave the Torre Serenissima a full upgrade to deliver more energy efficiency and comfort.
  • Van der Valk Hotel

    From the lobby to the guest rooms to the kitchen, every space in the Van der Valk Hotel has its own unique climate needs. Our goal was to develop an integrated system to meet the needs of each of these locations and lower the total environmental impact of the system.
  • Velocity office building

    Sustainability is at the forefront of Velocity's design. Each element of the design has been carefully considered to ensure an EPC rating of "B" and an "Excellent" BREEAM rating has been achieved.
  • Venetian Arsenal

    An innovative climate control system that taps into the natural energy of the Venetian Lagoon is delivering high levels of comfort and energy efficiencies while preserving an historic industrial building in the heart of Venice.
  • VMD business centre

    A VRV IV system is providing all the heating and cooling for VMD Tower B, a 25-storey office building in Zagreb, helping it to meet the highest levels of efficiency and lowering energy consumption.