Skip to main content

Radisson Blu and Proximus

Bruges, Belgium

The new Radisson Blue hotel in Bruges is located near Bruges station, an area which has seen extensive redevelopment over the past few years.

Built by Belgian property developer Group GL, the impressive new tower complex houses not only the new hotel but also a 6,000 square metre area of office space, currently occupied by GL tenant Proximus.

For the GL Group, finding a system that could provide optimal climate comfort and energy efficiency, while accommodating different functions within the building, posed a complex challenge.

Additionally, the Group sought a solution that could respond to potential changes in the building purpose or tenants over time.

The flexibility of Daikin’s VRV climate control system and GL’s previous experience of Daikin were key determinants in the Group’s choice, according to John Lenaers of Group GL.

Daikin is strong in the sector, with an excellent price/quality/service ratio...This is one of Daikin's strong points which, together with its acknowledged state-of-the-art technology, was a deciding factor for us.

 

“The system is particularly user-friendly and so easy to use. The modular system allows us to control multiple zones and thus accurately manage the climate of different floors and areas.”

John Lenaers - Group GL

Solution at a glance

bg-image

Lenaers notes the benefits of a modular system both in design terms and in shortening installation time:
Fast installation and aesthetics are tackled at the same time. Thanks to the simple design, the modules were integrated into the different spaces and are virtually undetectable. When in use, they provide a high degree of efficiency and comfort.

With the two businesses presenting different comfort and operational needs, flexibility is a must, as Lenaers observes:
The modular aspect is an added value. It means that we can divide and integrate the building into control zones, both for the Radisson hotel and for the Proximus offices. If the layout and/or function of the building changes in the future, Daikin will be able to meet this need seamlessly.

 

bg-image

A further advantage of the modular structure is that, in the event of malfunctioning or system shutdowns, partial control of the building is still possible.

Feedback from hotel guests on their climate experience in the hotel rooms has been positive, with the system’s silent operation and individual room control features particularly appreciated.

 

bg-image

From the tenant’s point of view, the Daikin VRV system has found widespread favour, with 80% of staff expressing satisfaction with the climate in the offices according to Denis Schelstraete, Proximus Facility Manager. He also stresses the advantage of the low noise system:

The complete soundproofing of the system is also important in office buildings where people often have to focus hard during their work or at meetings.

 

Learn more

Our other cases

  • Crystal Tower

    To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution.
  • Torre Serenissima

    Equipped with an outdated R-22 refrigerant system, we gave the Torre Serenissima a full upgrade to deliver more energy efficiency and comfort.
  • The Bloomsbury Hotel

    The VRVIII Heat Recovery System from Daikin was selected for its supremely low energy consumption and ability to off er massive savings in comparison with similar systems
  • VMD business centre

    A VRV IV system is providing all the heating and cooling for VMD Tower B, a 25-storey office building in Zagreb, helping it to meet the highest levels of efficiency and lowering energy consumption.
  • Velocity office building

    Sustainability is at the forefront of Velocity's design. Each element of the design has been carefully considered to ensure an EPC rating of "B" and an "Excellent" BREEAM rating has been achieved.
  • Leon's restaurant

    M&E contractor, Synecore, installed its first ‘invisible’ HVAC system, the Daikin VRV IV i-Series at Leon Restaurant, central London, to overcome tight space restrictions and achieve maximum climate control efficiency.