Skip to main content

Inverter technology by Daikin

Think Smart, Think Green, Think Daikin Inverter!

inverter technology

What is an INVERTER air conditioner? How does it work?

A conventional air conditioner operates at fixed speed: it delivers a fixed amount of cooling capacity via fixed compressor speed. An INVERTER air conditioner utilizes an intelligent advanced control that regulates precisely the compressor speed to constantly adjust delivered capacity to meet the desired room temperature. This smart technology guarantees a comfortable and stable temperature, with less energy consumption compared to a Non Inverter system.

 

Why do you need INVERTER in Middle East?

The amount of cooling (heating) capacity required depends on the outside temperature and the heat inside the room to be treated. Since the outside temperature varies all year long, but also during the course of the day, the cooling requirements will also vary all year round. Only a smart system – Inverter – can constantly adjust the delivered capacity to meet the specific requirements.

 

Benefits of INVERTER at a glance

> Energy saving all the year round, for a lower electricity bill and lower carbon footprint

> Powerful cooling

> Quieter operation

> Longer lifetime

 

Less energy use, for a lower electricity bill

The repeated ON/OFF operation of traditional systems leads to wasted energy consumption. With Daikin INVERTER, it constantly adjusts the compressor speed to precisely maintain the desired temperature, and contributes on reducing the energy consumption all year round, for a lower electricity bill.

By improving the real life efficiency and minimizing the use of energy, INVERTER systems reduce carbon footprint, for a lower impact on the environment.

 


Powerful cooling

The variable speed of the Inverter is responsible for the continuous adjustment of the capacity as needed without stopping its operation, for a maximized comfort with minimized temperature fluctuations. Traditional systems regulate the temperature by repeatedly starting and stopping the compressor, resulting in big temperature fluctuations and in a disturbing ON/OFF noise.

 

Also, Inverter reduces the system start-up time, so the required room temperature is reached much faster. With Daikin Inverter, the cooling is quick and powerful, even under high ambient conditions.

 

Quieter operation

The operation of Inverter is more silent compared to conventional air conditioner, and there is no disquieting ON/OFF noise.

Longer lifetime

The variable speed operation of Inverter allows an extended compressor lifetime against Non Inverter equipment. Non Inverter systems must repeatedly turn ON/OFF its compressor,resulting in a higher stress on the motor.

Energy Saving

Daikin offers efficient operation on its equipment for lower electricity consumption. This also contributes to reduce CO2 emissions.

Powerful Cooling

Rapid cooling and powerful, even if outside temperature is very high

Tropical Compressor

The tropical compressor is able to handle and operate fully under extreme weather conditions.

Silence

Daikin indoor units are whisper quiet. Outdoor units are also guaranteed not to disturb the quietness of the neighbourhood.

Learn More

Documentation